Introduction
These examples act as Modbus/TCP server devices, responding to requests from Modbus/TCP clients by serving data through standard Modbus registers such as coils, discrete inputs, input registers, and holding registers. By using the NanoModbus library, developers can create lightweight, efficient Modbus/TCP servers suitable for embedded systems with limited resources.
- The implementation consists of
- Modbus/TCP Stack
- NanoModbus Lib
- Ethernet Driver
- ENET CPSW
- LwIP TCP/IP networking stack with SNMP support on top of ethernet driver
- Modbus Server Application
Modbus/TCP Device Datasheet
Supported Modbus/TCP Functionality
| Feature | Description | Implementation |
| Modbus/TCP Protocol | Supports the Modbus/TCP protocol for communication between devices. | Yes |
| Modbus Function Codes | Supports a wide range of Modbus functions | Yes |
| Modbus/TCP Server | The stack supports being a Modbus/TCP Server. | Yes |
| Modbus/TCP Client | The stack supports being a Modbus/TCP Client. | No |
| Exception Handling | Supports exception handling for Modbus requests. | Yes |
| Data Integrity | Supports CRC and error checking mechanisms. | No |
| Modbus/TCP over Ethernet | The stack works over standard Ethernet interfaces for Modbus/TCP. | Yes |
| Timeout Handling | Supports configurable timeout values for Modbus transactions. | Yes |
| Secure Modbus/TCP (SSL/TLS) | Secure Modbus/TCP connections over SSL/TLS. | No |
| Modbus/TCP over NanoModbus | Support for using Modbus/TCP in a lightweight, optimized stack. | Yes |
Key Performance Parameters
| Feature | Detail | Value |
| Maximum Connections | Number of simultaneous Modbus TCP connections | 4 |
| Response Time | Average time to respond to a Modbus request (from client to server) | > 200ms |
| Error Detection and Recovery | Modbus CRC error detection and error recovery mechanisms | No |
| Max Data Length | Maximum Modbus TCP message length supported | 250 Bytes |
| Min Timeout Duration | Modbus TCP timeout duration | 10ms |
| Max Coils read per second | Maximum number of coils that can be read per second | 7957 coils |
| Max holding Registers read per second | Maximum number of registers(125) to be read per second | 986 registers |
| Max Coils write per second | Maximum number of coils(1000) to be written per second | 7986 coils |
| Max holding Registers write per second | Maximum number of registers(123) to be written per second | 979 registers |
| Max Coils write per second | Maximum number of coils (1000) that can be written per second | 7986 coils |
| Max Input Registers read per second | Maximum number of registers(125) to be read per second | 995 registers |
| Max discrete Inputs read per second | Maximum number of registers(1000) to be read per second | 7883 registers |
General Stack Parameters
Supported Function Codes
| Function Code | Description | Supported |
| 01 | Read Coils | Yes |
| 02 | Read Discrete Inputs | Yes |
| 03 | Read Holding Registers | Yes |
| 04 | Read Input Registers | Yes |
| 05 | Write Single Coil | Yes |
| 06 | Write Single Register | Yes |
| 15 | Write Multiple Coils | Yes |
| 16 | Write Multiple Registers | Yes |
Stack Memory Usage
| Demo Type | Code | RO Data | RW Data |
| Modbus Server CPSW | 201kB | 43,84kB | 437,20kB |
| Modbus Server ICSS | 184,68kB | 66,80kB | 697,97kB |
Steps to Run the Example
Build the example
HW Setup
- Note
- Make sure you have setup the EVM with cable connections as shown here, EVM Setup. In addition do below steps.
AM64X-EVM
- Connect an ethernet cable to the EVM from host PC as shown below
Ethernet cable for ICSS based ethernet
Ethernet cable for CPSW based ethernet
Run the example
- Attention
- If you need to reload and run the example again, EVM power-cycle is MUST.
- Launch a CCS debug session and run the example executable, see CCS Launch, Load and Run
- You will see logs in the UART terminal as shown in the next section.
- Note the IP address seen in the log, this is what we will use to communicate with the EVM.
- Open the Modbus tester tool, set the device’s IP address and port, and send Modbus requests, for instance request read holding register
UART Log
- The application shows a message New MODBUS client connected once a TCP client requests to connect.
Sample Output
==========================
CPSW LWIP TCP CLIENT
==========================
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 4 To 3
Open MAC port 1
EnetPhy_bindDriver:1935
PHY 3 is alive
PHY 12 is alive
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-0 : 70:ff:76:1f:d0:19
[0]Enet IF UP Event. Local interface IP:0.0.0.0
[LWIPIF_LWIP] Enet has been started successfully
[0]Enet IF UP Event. Local interface IP:192.168.0.200
Waiting for network UP ...
Waiting for network UP ...
Waiting for network UP ...
Cpsw_handleLinkUp:1616
MAC Port 1: link up
[0]Network Link UP Event
Network is UP ...
CPU load = 0 %
CPU load = 0 %
New MODBUS client connected 70099AA0
CPU load = 0 %
Communicate with the LP using ethernet
- Firstly you can try to reach the LP using ping as shown below, using a command shell on the host PC
> ping 192.168.0.200
Reference
- Modbus Application Protocol Specification, v1.1b3