Scope
This example demonstrates how to integrate an HTML webserver using the Ethernet over EtherCAT (EoE) mailbox protocol and LWIP. To learn more about EoE, please refer to the Ethernet over EtherCAT FAQ.
Related Files
LWIP
LWIP is a Lightweight TCP/IP stack written in ANSI C that provides the following features:
- IPv4 and IPv6 with UDP, TCP, ICMP and IGMP
- Ethernet and IPv4/IPv6 over IEEE 802.3
- DNS
- SNTP
- DHCP
- UDP and TCP SOCKET API
- IPv4 and IPv6 multicast
The LWIP project is distributed under the BSD-3-Clause license. The project can be downloaded here. It is also included in the MCU+SDK.
LWIP Settings
The LWIP settings for the Webserver Example can be found in the files located in the source/industrial_comms/ethercat_subdevice/stack/lwip/lwip-config/ directory:
- lwiphooks.h: Contains hooks into the LWIP stack that allow the application to interact with it.
- lwipopts.h: Contains configuration options for the LWIP stack to enable/disable features and optimize memory usage.
- lwippools.h: Contains memory pool definitions used by the LWIP stack for different protocols.
More information can be found in the official LWIP documentation. Changes to these files require a rebuild of the LWIP libraries using the provided makefile:
make -s -f makefile.amxxx.r5f
The resulting libraries will be placed in the /lib folder.
LWIP Debugging
LWIP debugging can be enabled in the lwipopts.h file by setting the LWIP_DEBUG macro to a non-zero value and configuring the debug level:
#define LWIP_DEBUG 1
#ifdef LWIP_DEBUG
#define LWIP_DBG_MIN_LEVEL LWIP_DBG_LEVEL_ALL
#define PPP_DEBUG LWIP_DBG_ON
#define MEM_DEBUG LWIP_DBG_ON
#define MEMP_DEBUG LWIP_DBG_ON
#endif
Webserver Example Implementation
The Webserver example extends the Simple example by creating:
- A dedicated webserver thread that initializes and runs the HTTP server
- EoE callback handlers for processing incoming Ethernet frames and network settings
- LWIP integration for webserver functionality
- EoE APIs for handling EoE settings and messages
After running the application and configuring TwinCAT (or another EoE-capable MainDevice), you can connect to the webserver by entering the SubDevice's IP address in a web browser. The server supports three different pages:
- Main page (xxx.xxx.xxx.xxx/main.html): Displays a simple welcome page
- Favicon (xxx.xxx.xxx.xxx/favicon.ico): Shows a small Texas Instruments logo
- 404 Error: Displayed for any other requested URL
Implementation Overview
The EoE implementation consists of two main components:
- EoE callback handlers registered in the main application that process incoming EoE frames
- A dedicated webserver task that initializes the network interface and handles HTTP requests
EC_SLV_APP_SS_loopTask
The main application task registers the EoE callbacks:
- EC_API_SLV_EoE_cbRegisterReceiveHandler: Registers the
EC_SLV_APP_EoE_SS_receiveHandler function, which is called when an EoE message with an Ethernet frame is received. The function passes the Ethernet frame to the LWIP network interface for processing.
{
LOCK_TCPIP_CORE();
struct pbuf *p = pbuf_alloc(PBUF_RAW, size, PBUF_POOL);
DebugP_assert(p != NULL);
pbuf_take(p, (const void *)pData, size);
if (gnetif.input(p, &gnetif) != ERR_OK)
{
pbuf_free(p);
p = NULL;
}
UNLOCK_TCPIP_CORE();
return true;
}
bool EC_SLV_APP_EoE_SS_receiveHandler(void *pContext, uint16_t *pData, uint16_t size)
User defined EoE receive function. Called when an EoE frame is received.
Definition ESL_eoeDemo.c:565
- EC_API_SLV_EoE_cbRegisterSettingIndHandler: Registers the
EC_SLV_APP_EoE_SS_settingIndHandler function, which is called when an EoE message with network settings is received. The function applies the received settings to the LWIP network interface.
{
ip4_addr_t ip;
ip4_addr_t subnet;
ip4_addr_t gateway;
ip4_addr_t dns;
eoeContext_s.settingsReceived = 1;
if (pMac != NULL && (pMac[0] | pMac[1] | pMac[2]) != 0)
{
gnetif.hwaddr[0] = pMac[0] >> 8;
gnetif.hwaddr[1] = pMac[0] & 0xFF;
gnetif.hwaddr[2] = pMac[1] >> 8;
gnetif.hwaddr[3] = pMac[1] & 0xFF;
gnetif.hwaddr[4] = pMac[2] >> 8;
gnetif.hwaddr[5] = pMac[2] & 0xFF;
}
IP4_ADDR(&ip,
pIp[0] & 0xFF, pIp[0] >> 8,
pIp[1] & 0xFF, pIp[1] >> 8);
IP4_ADDR(&subnet,
pSubNet[0] & 0xFF, pSubNet[0] >> 8,
pSubNet[1] & 0xFF, pSubNet[1] >> 8);
IP4_ADDR(&gateway,
pDefaultGateway[0] & 0xFF, pDefaultGateway[0] >> 8,
pDefaultGateway[1] & 0xFF, pDefaultGateway[1] >> 8);
IP4_ADDR(&dns,
pDnsIp[0] & 0xFF, pDnsIp[0] >> 8,
pDnsIp[1] & 0xFF, pDnsIp[1] >> 8);
LOCK_TCPIP_CORE();
netif_set_addr(&gnetif, &ip, &subnet, &gateway);
UNLOCK_TCPIP_CORE();
return true;
}
bool EC_SLV_APP_EoE_SS_settingIndHandler(void *pContext, uint16_t *pMac, uint16_t *pIp, uint16_t *pSubNet, uint16_t *pDefaultGateway, uint16_t *pDnsIp)
EoE Settings Indication callback. Called when EoE settings are received.
Definition ESL_eoeDemo.c:482
EC_SLV_APP_EoE_SS_Task
The webserver task performs the following steps:
- Network Interface Initialization: Initializes the virtual network interface with
netif_if_init()
- Creates a semaphore for LWIP initialization
- Initializes the TCP/IP stack with
tcpip_init()
- Adds the network interface with
netif_add()
- Configures the interface with MAC address, ARP handling, and output function
- Webserver Initialization: Sets up the HTTP server with
EC_SLV_APP_EoE_SS_initializeWebserver()
- Creates a socket with
socket()
- Binds the socket to port 80 with
bind()
- Starts listening for connections with
listen()
- HTTP Request Handling: Enters a loop to process incoming connections
- Accepts connections with
accept()
- Receives data with
recv()
- Processes GET requests with
EC_SLV_APP_EoE_SS_WebSrvProcessGetAndRespond()
- Sends appropriate responses based on the requested URL
- Closes the connection with
shutdown() and close()
Frame Handling Flow
When an EoE frame is received:
- The EtherCAT stack invokes the registered callback
EC_SLV_APP_EoE_SS_receiveHandler
- The callback allocates a LWIP packet buffer and copies the frame data
- The frame is passed to the LWIP stack via
gnetif.input()
- LWIP processes the frame according to the protocol (TCP/IP, UDP, etc.)
- For HTTP requests, the webserver task handles the incoming connection
Thread Safety
The EoE implementation uses LOCK_TCPIP_CORE() and UNLOCK_TCPIP_CORE() macros to ensure thread safety when accessing the LWIP stack. These macros protect critical sections of code that interact with the network interface.
Error Handling
The EoE implementation includes robust error handling for network operations:
EC_SLV_APP_EoE_SS_WebSrvStrError() converts error codes to human-readable strings
EC_SLV_APP_EoE_SS_WebSrvIsFatalErr() distinguishes between fatal and non-fatal errors
- Error conditions are logged for debugging purposes
MAC Address Management
The EoE implementation can use MAC addresses from different sources:
- MAC address received from the EtherCAT MainDevice via EoE settings
- MAC address stored in EEPROM (retrieved using EC_SLV_APP_EEP_getMacAddress)
- Default MAC address (all zeros) if other sources are unavailable
Debugging
The source code contains debug print statements that can be enabled by defining the EOE_DEBUG_PRINTS macro in ESL_eoeDemo.h. These prints provide detailed information about:
- EoE message reception and processing
- Network interface initialization
- Webserver operation and connections
- Error conditions and handling
Testing and Troubleshooting
When testing the EoE functionality, consider the following:
- Ensure that the EtherCAT MainDevice is configured to support EoE
- Verify that the IP address, subnet mask, and gateway settings are correct
- Use Wireshark to capture and analyze EoE traffic with these useful filters:
- ecat_mailbox.eoe (EoE Fragment)
- ecat_mailbox.eoe.fragment (EoE Fragment Header)
- ecat_mailbox.eoe.fraghead (EoE Fragment Data)
For more filters, refer to the Wireshark EtherCAT Mailbox Filter Reference.
Common issues include:
- Incorrect network settings
- Firewall blocking connections
- MAC address conflicts
- Insufficient memory for LWIP buffers