EtherCAT SubDevice
 
Loading...
Searching...
No Matches
Setup

Software installation

for details see Getting started

Connect the development board

TMDS243GPEVM/TMDS64GPEVM

Board details: TMDS64EVM, TMDS243EVM

  1. Setup a dip switches on the board : 25MHz, No-boot / Dev-boot.
No boot mode
  1. Connect the evaluation board to your computer using the micro-USB cables.

    One USB cables is required for the JTAG interface (XDS110), a second cable for the UART console.

USB connectors on the AM64x/AM243 GP EVM Board
  1. Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
EtherCAT ports
  1. If you have multiple devices in chain, please connect from EtherCAT OUT/Port1 to IN/Port0 of next device. For the last device in chain, OUT/Port1 will be left open (if NOT using redundancy mode).
  2. Connect the board(s) to the power supply(ies) according to the specifications in the AM64x/AM243x GP EVM User's Guide Rev D

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu , see Using SDK with CCS Projects
  • When using makefiles to build, note the required combination and build using make command , see Using SDK with Makefiles