PROFINET Device4.0.3
 
Loading...
Searching...
No Matches
Introduction

This is the integration manual of the PROFINET® Device stack on Sitara™ AM64x Platform. The PROFINET stack is executed on a dedicated R5F Core running FreeRTOS.


Note
The PROFINET stack could only be used with SOC_AM64xx and SOC_AM243x type "F", usage with other chip types may be subject of faulty behavior!

The demo application was built with:

  • Code Composer Studio Version: 12.7.0
  • SysConfig v1.20.0
  • INDUSTRIAL-COMMUNICATIONS-SDK for AM64x v09.02
  • TI Arm Clang Compiler 3.2.2.LTS

The latest testresult of the ART can be found here: art_testreport.pdf

The latest testresult of the SPIRTA can be found here: SPIRTA_Result