|
AM64x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
54 #ifndef RM_TISCI_IRQ_H
55 #define RM_TISCI_IRQ_H
68 #define TISCI_MSG_VALUE_RM_DST_ID_VALID (1u << 0u)
73 #define TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID (1u << 1u)
78 #define TISCI_MSG_VALUE_RM_IA_ID_VALID (1u << 2u)
83 #define TISCI_MSG_VALUE_RM_VINT_VALID (1u << 3u)
88 #define TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID (1u << 4u)
93 #define TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID (1u << 5u)
uint16_t src_index
Definition: tisci_rm_irq.h:206
uint16_t dst_host_irq
Definition: tisci_rm_irq.h:338
uint16_t vint
Definition: tisci_rm_irq.h:340
uint16_t dst_id
Definition: tisci_rm_irq.h:337
uint32_t valid_params
Definition: tisci_rm_irq.h:334
uint16_t dst_host_irq
Definition: tisci_rm_irq.h:208
uint16_t global_event
Definition: tisci_rm_irq.h:341
uint16_t src_id
Definition: tisci_rm_irq.h:205
Configures peripherals within the interrupt subsystem according to the valid configuration provided....
Definition: tisci_rm_irq.h:202
uint8_t vint_status_bit_index
Definition: tisci_rm_irq.h:212
uint16_t dst_id
Definition: tisci_rm_irq.h:207
uint16_t global_event
Definition: tisci_rm_irq.h:211
struct tisci_header hdr
Definition: tisci_rm_irq.h:203
uint16_t vint
Definition: tisci_rm_irq.h:210
struct tisci_header hdr
Definition: tisci_rm_irq.h:223
uint16_t src_index
Definition: tisci_rm_irq.h:336
struct tisci_header hdr
Definition: tisci_rm_irq.h:353
uint32_t valid_params
Definition: tisci_rm_irq.h:204
struct tisci_msg_rm_irq_set_req __attribute__((__packed__))
uint16_t ia_id
Definition: tisci_rm_irq.h:209
Response to setting a peripheral to processor interrupt.
Definition: tisci_rm_irq.h:222
uint16_t ia_id
Definition: tisci_rm_irq.h:339
uint8_t secondary_host
Definition: tisci_rm_irq.h:213
uint8_t secondary_host
Definition: tisci_rm_irq.h:343
struct tisci_header hdr
Definition: tisci_rm_irq.h:333
Response to releasing a peripheral to processor interrupt.
Definition: tisci_rm_irq.h:352
Releases interrupt peripheral resources according to the valid configuration provided....
Definition: tisci_rm_irq.h:332
uint16_t src_id
Definition: tisci_rm_irq.h:335
uint8_t vint_status_bit_index
Definition: tisci_rm_irq.h:342