- Note
- This example demostrates handling the ESM error in the Main domain R5. The error can also be routed to MCU ESM and error handled in the safety domain (M4 core)
Introduction
This example simulates a 1b and 2b ECC error for DDR and waits for interrupt via the MAIN ESM instance. If the interrupt is not received the test fails.
Supported Combinations
AM64X
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am64x-evm am64x-sk |
Example folder | examples/drivers/ddr/ddr_ecc_test_main_esm/ |
Steps to Run the Example
See Also
DDR
Sample Output
Shown below is a sample output when the application is run,
Waiting on Single bit Error Correction Interrupt...
1b ECC error detected and corrected
Waiting on Dual bit error detection Interrupt...
2b ECC error detected
All tests have passed!!