AM64x INDUSTRIAL COMMUNICATIONS SDK  09.00.00
EtherCAT-IOLink Gateway Demo

Introduction

This example is an EtherCAT-IOLink Gateway application based on evaluation stack provided in the SDK. Links to important sections in the detailed documentation are provided below:

Attention
If you need to reload and run the example again, EVM power-cycle is MUST.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSG ICSSG0 and ICSSG1
Toolchain ti-arm-clang
Board am64x-evm
Example folder examples/industrial_comms/ethercat_iolink_gateway_demo