Enumeration types can be defined in the Object Dictionary and these are hidden in the index range between 0x0800 and 0x0FFF. Enumeration type entries are composed by a value and by a name. Moreover, the enum bit size has to be provided. To create and configure the enumeration, these API functions are available: EC_API_SLV_CoE_odAddEnum and EC_API_SLV_CoE_configEnum.
Create and configure the new ENUM type
Use the function EC_API_SLV_CoE_odAddEnum to create the enum object. As input parameter it requires the SDK handle and the enumeration index. The index must be between 0x0800 and 0x0FFF, otherwise it will return an error code. The output parameter in an OBD object.
#define SLS_OBJIDX_FSOE_CONN_STATE 0x0800
{
OSAL_printf("Object SLS_OBJIDX_FSOE_CONN_STATE Error code: 0x%08x\r\n", error);
}
@ EC_API_eERR_NONE
Definition ecSlvApi_Error.h:45
enum EC_API_EError EC_API_EError_t
uint32_t EC_API_SLV_CoE_odAddEnum(EC_API_SLV_SHandle_t *ecSlaveApi, uint16_t index, EC_API_SLV_SCoE_Object_t **outObject)
This function creates an ENUM Object.
Definition ecSlvApi_CoEStub.c:958
Use the function EC_API_SLV_CoE_configEnum to configure each enum entry. As input parameters, it requires the SDK handle, the enumeration object and then the entry value and entry name.
#define FSOE_CONN_ST_RESET 100
#define FSOE_CONN_ST_SESSION 101
#define FSOE_CONN_ST_CONNECTION 102
#define FSOE_CONN_ST_PARAMETER 103
#define FSOE_CONN_ST_DATA 104
#define FSOE_CONN_ST_FAILSAFE 105
uint32_t EC_API_SLV_CoE_configEnum(EC_API_SLV_SHandle_t *ecSlaveApi, EC_API_SLV_SCoE_Object_t *object, uint32_t value, char *name)
This function creates an ENUN Object.
Definition ecSlvApi_CoEStub.c:998
Using the new ENUM type
The new enumeration type can now be used as type parameter for variable, array and record objects. Provide the enumeration index as type parameter and specify the enumeration bit length. The enumeration size can be up to 32 bits.
#define SLS_OBJIDX_FSOE_DIG_IO_MODULE 0xA000
#define SLS_OBJIDX_FSOE_CONN_STATE 0x0800
SLS_OBJIDX_FSOE_DIG_IO_MODULE,
"FSoE Digital IO Module",
NULL,
NULL,
NULL,
NULL,
&pApplicationInstance->ptA000RecObj);
pApplicationInstance->ptA000RecObj,
1,
"Connection State",
SLS_OBJIDX_FSOE_CONN_STATE,
16,
{
OSAL_printf("Object 0xA000 SubIndex 1 Error code: 0x%08x\r\n", error);
goto Exit;
}
uint32_t EC_API_SLV_CoE_configRecordSubIndex(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint8_t subIndex_p, char *pName_p, uint16_t type_p, uint16_t bitLen_p, uint16_t flags_p)
This function creates a subIndex for the Record Object.
Definition ecSlvApi_CoEStub.c:922
uint32_t EC_API_SLV_CoE_odAddRecord(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t index_p, char *pName_p, EC_API_SLV_CBObjRead_t cbRead_p, void *pReadCtxt_p, EC_API_SLV_CBObjWrite_t cbWrite_p, void *pWriteCtxt_p, EC_API_SLV_SCoE_Object_t **pOutSdo_p)
This function creates a Record Object.
Definition ecSlvApi_CoEStub.c:867
#define ACCESS_READ
Read only in all states.
Definition ecSlvApiDef_CoE.h:149
Finally set a value after initializing the stack with the EC_API_SLV_init.
uint16_t connectionState = FSOE_CONN_ST_RESET;
uint32_t EC_API_SLV_CoE_getObjectEntryByObject(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint8_t subIndex_p, EC_API_SLV_SCoE_ObjEntry_t **ppObjectEntry_p)
This function returns object entries from the Object Dictionary.
Definition ecSlvApi_CoEStub.c:473
uint32_t EC_API_SLV_CoE_setObjectEntryData(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_ObjEntry_t *pObjectEntry_p, uint32_t length_p, uint16_t *pData_p)
This function writes Data to the Object Dictionary.
Definition ecSlvApi_CoEStub.c:639
Enumeration in TwinCAT
The enumeration subIndex can now be accessed by TwinCAT.
A000 object with subIndex 1 of enumeration type
|
td |
The data dialog window shows a box with all possible enumeration values.
Enumeration box in TwinCAT
|
td |