![Logo](ti_logo.svg) |
AM263x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
54 #define RTS_TEXT_SECTION __attribute__((section(".trigText"))) __attribute__((always_inline))
55 #define RTS_DATA_SECTION __attribute__((aligned(8), section(".trigData")))
136 __asm (
"VSQRT.F32 %0, %1" :
"=t" (r) :
"t" (x));
void FastRTS_sincos(const float theta, float *retValues)
The Sine/Cosine Function.
float FastRTS_logf(const float x)
The Natural Logarithm function.
float FastRTS_expf(const float x)
The Exponent function.
float FastRTS_cosf(const float theta)
The Cosine Function.
#define RTS_TEXT_SECTION
Definition: fastrts.h:54
float FastRTS_acosf(const float theta)
The Arccosine Function.
float FastRTS_atan2f(const float y, const float x)
The Arctangent(y,x) function.
static RTS_TEXT_SECTION float FastRTS_sqrtf(const float x)
Definition: fastrts.h:133
float FastRTS_sinf(const float theta)
The Sine Function.
float FastRTS_atanf(const float x)
The Arctangent function.
float FastRTS_asinf(const float theta)
The Arcsine Function.