AM263x MCU+ SDK  09.00.00
EQEP frequency measurement

Introduction

This example uses the EQEP to measure frequency of a signal generated by ePWM.

Figure 1a. Block diagram

The example does the below

  • Configures EPWM to generate a signal and EQEP to measure frequency of this generated signal (a loopback connection is required).
  • The application runs for the specified time and the frequency calculation is done using the EPWM ISR.
  • After the specified time, the application checks if the measured frequency was within range of the generated frequency.

Figure 1b. Implementation details

External connections

  • Connect ePWM0A to eQEP0A (EPWM simulates eQEP signal)

AM263X-CC

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Connect HSEC Pin 49 (ePWM0A) to HSEC Pin 102 (eQEP0A)

AM263X-LP

  • Connect J2 Pin 11 (ePWM0A) to J25 Pin 1 (eQEP0A)

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc, am263x-lp
Example folder examples/drivers/eqep/eqep_frequency_measurement/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • View the UART console logs for results

See Also

EQEP

Sample Output

Shown below is a sample output when the application is run,

EQEP Frequency Measurement Test Started ...
Please ensure EPWM to EQEP loopback is connected...
Please wait 10 seconds ...
Expected frequency = 10000 Hz, Measured frequency = 10000 Hz
EQEP Frequency Measurement Test Passed!!
All tests have passed!!