AM263Px INDUSTRIAL COMMUNICATIONS SDK  2026.00.00

Detailed Description

GPIO enable configuration with PRU direct access.

Configuration for TX enable pin that the PRU firmware controls directly via physical memory access for precise timing control.

Data Fields

IOLFW_GpioConfig_t gpio
 
uint32_t gpioPhysAddr
 
uint32_t gpioPinMask
 

Field Documentation

◆ gpio

IOLFW_GpioConfig_t IOLFW_GpioEnConfig_t::gpio

Base GPIO configuration

◆ gpioPhysAddr

uint32_t IOLFW_GpioEnConfig_t::gpioPhysAddr

Physical address for PRU direct GPIO access

◆ gpioPinMask

uint32_t IOLFW_GpioEnConfig_t::gpioPinMask

Bit mask for the GPIO pin