AM263Px INDUSTRIAL COMMUNICATIONS SDK  2026.00.00

Introduction

Functions

void PN_event1IsrHandler (void *arg)
 Event1 ISR handler. Used to call the application ISR Handler in case a Ti ISOM event/signal is triggered. More...
 
void PN_event2IsrHandler (void *arg)
 Event2 ISR handler. Used to call the application ISR Handler in case a To ISOM event/signal is triggered. More...
 
int8_t PN_ISO_initGPIOEvent (PN_Handle pnHandle, uint8_t isoMode, uint8_t isoEvent, uint32_t timeval, uint32_t duration)
 API to initialize the ISOM event/signal. Returns the ISOM handle. The Event/signal will be disabled by default. More...
 
void PN_ISO_enableGPIOEvent (PN_Handle pnHandle)
 API to enable the ISOM event/signal generation. More...
 
void PN_ISO_disableGPIOEvent (PN_Handle pnHandle)
 API to disable the ISOM event/signal generation. More...
 
void PN_ISO_deInitGPIOEvent (PN_Handle pnHandle)
 API to De init the ISOM event/signal. More...
 

Macros

#define PNISO_MAX_NUM_EVENTS   2
 
#define PNISO_MODE_NONE   0
 
#define PNISO_MODE_INTERRUPT   1
 
#define PNISO_MODE_GPIO   2
 
#define PNISO_MODE_DISABLE   0
 
#define PNISO_MODE_ENABLE   1
 
#define PNISO_TI_EVENT   1
 
#define PNISO_TI_EVENT_REG_SHIFT   0
 
#define PNISO_TO_EVENT   2
 
#define PNISO_TO_EVENT_REG_SHIFT   1
 
#define PNISO_ERR_SUCCESS   0
 
#define PNISO_ERR_INVALID_EVENT   -1
 
#define PNISO_ERR_EVENTS_EXHAUSTED   -2
 

Macro Definition Documentation

◆ PNISO_MAX_NUM_EVENTS

#define PNISO_MAX_NUM_EVENTS   2

Maximum number of ISOM events supported in a network cycle by firmware

◆ PNISO_MODE_NONE

#define PNISO_MODE_NONE   0

Used to Disable ISOM mode

◆ PNISO_MODE_INTERRUPT

#define PNISO_MODE_INTERRUPT   1

ISOM Interrupt Mode

◆ PNISO_MODE_GPIO

#define PNISO_MODE_GPIO   2

ISOM GPIO Mode

◆ PNISO_MODE_DISABLE

#define PNISO_MODE_DISABLE   0

Disable ISOM mode

◆ PNISO_MODE_ENABLE

#define PNISO_MODE_ENABLE   1

Enable ISOM mode

◆ PNISO_TI_EVENT

#define PNISO_TI_EVENT   1

Input ISOM event

◆ PNISO_TI_EVENT_REG_SHIFT

#define PNISO_TI_EVENT_REG_SHIFT   0

Bit shift value for TI event

◆ PNISO_TO_EVENT

#define PNISO_TO_EVENT   2

Output ISOM event

◆ PNISO_TO_EVENT_REG_SHIFT

#define PNISO_TO_EVENT_REG_SHIFT   1

Bit shift value for TO event

◆ PNISO_ERR_SUCCESS

#define PNISO_ERR_SUCCESS   0

◆ PNISO_ERR_INVALID_EVENT

#define PNISO_ERR_INVALID_EVENT   -1

◆ PNISO_ERR_EVENTS_EXHAUSTED

#define PNISO_ERR_EVENTS_EXHAUSTED   -2

Function Documentation

◆ PN_event1IsrHandler()

void PN_event1IsrHandler ( void *  arg)

Event1 ISR handler. Used to call the application ISR Handler in case a Ti ISOM event/signal is triggered.

Parameters
[in]arg

◆ PN_event2IsrHandler()

void PN_event2IsrHandler ( void *  arg)

Event2 ISR handler. Used to call the application ISR Handler in case a To ISOM event/signal is triggered.

Parameters
[in]arg

◆ PN_ISO_initGPIOEvent()

int8_t PN_ISO_initGPIOEvent ( PN_Handle  pnHandle,
uint8_t  isoMode,
uint8_t  isoEvent,
uint32_t  timeval,
uint32_t  duration 
)

API to initialize the ISOM event/signal. Returns the ISOM handle. The Event/signal will be disabled by default.

Parameters
pnHandleProfinet Handle
[in]isoModeISOM Mode - PNISO_MODE_GPIO/PNISO_MODE_INTERRUPT
[in]isoEventISOM Event - PNISO_TI_EVENT/PNISO_TO_EVENT
[in]timevaltime in nanosecond to trigger the event/signal (Reference is Start of Cycle)
[in]durationDuration of signal in nanoseconds
Return values
0on success
-1if max number of events reached
-2if invalid event type passed

◆ PN_ISO_enableGPIOEvent()

void PN_ISO_enableGPIOEvent ( PN_Handle  pnHandle)

API to enable the ISOM event/signal generation.

Parameters
pnHandleProfinet Handle

◆ PN_ISO_disableGPIOEvent()

void PN_ISO_disableGPIOEvent ( PN_Handle  pnHandle)

API to disable the ISOM event/signal generation.

Parameters
pnHandleProfinet Handles

◆ PN_ISO_deInitGPIOEvent()

void PN_ISO_deInitGPIOEvent ( PN_Handle  pnHandle)

API to De init the ISOM event/signal.

Parameters
pnHandleProfinet Handle