Functions | |
| void | EIP_drvInit (EIP_Handle icssEipHandle) |
| Initialization routine for Ethernet/IP driver functions. More... | |
| void | EIP_drvStop (EIP_Handle icssEipHandle) |
| EIP driver stop API. More... | |
| void | EIP_drvStart (EIP_Handle icssEipHandle) |
| EIP driver start API. More... | |
| void | EIP_processProtocolFrames (uint32_t *queue_number, void *userArg) |
| API to process the real time Packets. More... | |
| int8_t | EIP_initializeCIPSync (EIP_Handle icssEipHandle) |
| API to initialize the CIP Sync objects in the EIP handle Initialize CIP Sync member variables based on PTP implementation. More... | |
| int32_t | EIP_configureLLDPForwarding (EIP_Handle icssEipHandle, uint8_t enableFeature) |
| API to configure the LLDP forwarding to the other port. More... | |
| int32_t | EIP_configureLLDPFwdHelper (uint32_t pruBaseAddress, uint8_t val) |
| API to configure the value stored at the required offset in ICSS SMEM. More... | |
| int32_t | EIP_configurePortForwarding (EIP_Handle icssEipHandle, uint8_t portNo, uint8_t portFwdState) |
| API to configure port forwarding state. More... | |
| int32_t | EIP_portFwdCtrlHelper (uint32_t pruBaseAddress, uint8_t portNo, uint8_t portFwdState) |
| Helper API to configure port forwarding state. More... | |
| void EIP_drvInit | ( | EIP_Handle | icssEipHandle | ) |
Initialization routine for Ethernet/IP driver functions.
This API does the following functionalities:
Loads the firmware on PRU0 and PRU1 cores
Call DLR init API
Call TimeSync(PTP) init API
| icssEipHandle | [in] EIP handle |
| void EIP_drvStop | ( | EIP_Handle | icssEipHandle | ) |
EIP driver stop API.
This API stops DLR and disables PTP
| icssEipHandle | [in] EIP handle |
| void EIP_drvStart | ( | EIP_Handle | icssEipHandle | ) |
EIP driver start API.
This API starts DLR and enables PTP
| icssEipHandle | [in] EIP handle |
| void EIP_processProtocolFrames | ( | uint32_t * | queue_number, |
| void * | userArg | ||
| ) |
API to process the real time Packets.
This API will be registered as Real Tme Rx Call back. Incase of EIP, the driver
receives DLR and PTP packets. This API receives the packet, checks the packet
type and passes the packet to DLR driver or PTP driver
| queue_number | [in] Queue where the packet is present |
| userArg | [in] userArgumment. EIP handle |
| int8_t EIP_initializeCIPSync | ( | EIP_Handle | icssEipHandle | ) |
API to initialize the CIP Sync objects in the EIP handle Initialize CIP Sync member variables based on PTP implementation.
| icssEipHandle | [in] EIP handle |
| 0 | - On success <0 - On failure |
| int32_t EIP_configureLLDPForwarding | ( | EIP_Handle | icssEipHandle, |
| uint8_t | enableFeature | ||
| ) |
API to configure the LLDP forwarding to the other port.
| icssEipHandle | [in] EIP handle |
| enableFeature | [in] Option to enable or disable the LLDP forwarding 1 - Feature is enabled 0 - Feature is disabled |
| 0 | - On success <0 - On failure |
| int32_t EIP_configureLLDPFwdHelper | ( | uint32_t | pruBaseAddress, |
| uint8_t | val | ||
| ) |
API to configure the value stored at the required offset in ICSS SMEM.
| pruBaseAddress | [in] PRU Base Address |
| val | [in] Value to program at the SMEM address |
| 0 | - On success <0 - On failure |
| int32_t EIP_configurePortForwarding | ( | EIP_Handle | icssEipHandle, |
| uint8_t | portNo, | ||
| uint8_t | portFwdState | ||
| ) |
API to configure port forwarding state.
| icssEipHandle | [in] EIP handle |
| portNo | [in] Port number (ICSS_EMAC_PORT_1 or ICSS_EMAC_PORT_2) |
| portFwdState | [in] Port forwarding state ICSS_EMAC_IOCTL_PORT_FWD_CTRL_ENABLE_CMD - Enable port forwarding ICSS_EMAC_IOCTL_PORT_FWD_CTRL_DISABLE_CMD - Disable port forwarding |
| 0 | - On success <0 - On failure |
| int32_t EIP_portFwdCtrlHelper | ( | uint32_t | pruBaseAddress, |
| uint8_t | portNo, | ||
| uint8_t | portFwdState | ||
| ) |
Helper API to configure port forwarding state.
| pruBaseAddress | [in] PRU Base Address |
| portNo | [in] Port number (ICSS_EMAC_PORT_1 or ICSS_EMAC_PORT_2) |
| portFwdState | [in] Port forwarding state ICSS_EMAC_IOCTL_PORT_FWD_CTRL_ENABLE_CMD - Enable port forwarding ICSS_EMAC_IOCTL_PORT_FWD_CTRL_DISABLE_CMD - Disable port forwarding |
| 0 | - On success <0 - On failure |