AM263Px INDUSTRIAL COMMUNICATIONS SDK  2026.00.00

Introduction

Functions

void RedProtocolInit (void)
 Assigns key function pointers based on macro. More...
 
void RedNodeTableClear (hsrPrpHandle *hsrPrphandle)
 Sets Clear Node Table flag to be used by PRU. More...
 
void RedIncrementCounter (uint32_t offset, PRUICSS_Handle pruicssHandle)
 Increments statistics counter. More...
 
void RedSupFrameUpdateTlv (hsrPrpHandle *hsrPrphandle, uint8_t type)
 
int32_t RedTxPacket (void *icssEmachandle, ICSS_EMAC_TxArgument *txArg, void *userArg)
 Enqueues redundancy frames to transmit. More...
 
int32_t RedRxPktGet (void *icssEmachandle, ICSS_EMAC_RxArgument *rxVoidArg, void *userArg)
 Copies data from L3 receive queues. More...
 
RED_STATUS RedLifeCheckTaskCreate (hsrPrpHandle *hsrPrphandle, PRUICSS_Handle pruicssHandle)
 Function to create RED Supervision task. More...
 
void RedLifeCheckTaskDelete (hsrPrpHandle *hsrPrphandle)
 Function to delete RED Supervision task. More...
 
RED_STATUS RedProtocolStart (hsrPrpHandle *hsrPrphandle, PRUICSS_Handle pruicssHandle)
 Function to start RedProtocolStart. More...
 
void RedProtocolConfigure (PRUICSS_Handle pruicssHandle)
 Configure IEP to modify max frame size (to acccount for LRE header) More...
 
void RedProtocolStop (hsrPrpHandle *hsrPrphandle, PRUICSS_Handle pruicssHandle)
 Delete Node Table check Task. More...
 

Function Documentation

◆ RedProtocolInit()

void RedProtocolInit ( void  )

Assigns key function pointers based on macro.

◆ RedNodeTableClear()

void RedNodeTableClear ( hsrPrpHandle *  hsrPrphandle)

Sets Clear Node Table flag to be used by PRU.

Parameters
hsrPrphandle

◆ RedIncrementCounter()

void RedIncrementCounter ( uint32_t  offset,
PRUICSS_Handle  pruicssHandle 
)

Increments statistics counter.

Parameters
offsetCounter
pruicssHandlePointer to PRU ICSS Handle, parent structure containing all switch information

◆ RedSupFrameUpdateTlv()

void RedSupFrameUpdateTlv ( hsrPrpHandle *  hsrPrphandle,
uint8_t  type 
)

◆ RedTxPacket()

int32_t RedTxPacket ( void *  icssEmachandle,
ICSS_EMAC_TxArgument *  txArg,
void *  userArg 
)

Enqueues redundancy frames to transmit.

Parameters
icssEmachandle
txArg
userArg
Returns
RED_OK on success, RED_ERR otherwise

◆ RedRxPktGet()

int32_t RedRxPktGet ( void *  icssEmachandle,
ICSS_EMAC_RxArgument *  rxVoidArg,
void *  userArg 
)

Copies data from L3 receive queues.

Parameters
icssEmachandle
rxVoidArg
userArg
Returns
RED_OK(0) on success, RED_ERR(1) otherwise

◆ RedLifeCheckTaskCreate()

RED_STATUS RedLifeCheckTaskCreate ( hsrPrpHandle *  hsrPrphandle,
PRUICSS_Handle  pruicssHandle 
)

Function to create RED Supervision task.

Parameters
hsrPrphandle
pruicssHandlePointer to PRU ICSS Handle, parent structure containing all switch information
Returns
RED_OK(0) if success, RED_ERR(1) otherwise

◆ RedLifeCheckTaskDelete()

void RedLifeCheckTaskDelete ( hsrPrpHandle *  hsrPrphandle)

Function to delete RED Supervision task.

Parameters
hsrPrphandle

◆ RedProtocolStart()

RED_STATUS RedProtocolStart ( hsrPrpHandle *  hsrPrphandle,
PRUICSS_Handle  pruicssHandle 
)

Function to start RedProtocolStart.

Parameters
hsrPrphandle
pruicssHandlePointer to PRU ICSS Handle, parent structure containing all switch information

◆ RedProtocolConfigure()

void RedProtocolConfigure ( PRUICSS_Handle  pruicssHandle)

Configure IEP to modify max frame size (to acccount for LRE header)

Parameters
pruicssHandlePointer to PRU ICSS Handle, parent structure containing all switch information

◆ RedProtocolStop()

void RedProtocolStop ( hsrPrpHandle *  hsrPrphandle,
PRUICSS_Handle  pruicssHandle 
)

Delete Node Table check Task.

Parameters
hsrPrphandle
pruicssHandlePointer to PRU ICSS Handle, parent structure containing all switch information