AM263Px INDUSTRIAL COMMUNICATIONS SDK  2026.00.00
IO-Link Master Demo

Introduction

This example is an IO-Link Master application based on evaluation stack provided in the SDK. Links to important sections in the detailed documentation are provided below:

IO-Link Master GUI Tool can be downloaded from here.

Attention
If you need to reload and run the example again, EVM power-cycle is MUST.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSM ICSSM0
Toolchain ti-arm-clang
Board am263px-lp
Example folder examples/industrial_comms/iolink_master_demo