AM261x INDUSTRIAL COMMUNICATIONS SDK  2026.00.00
Introduction

Welcome to Industrial Communications SDK for AM261X. This SDK contains examples, libraries and tools to develop RTOS based Industrial Communication applications on PRU-ICSS.

The Industrial Communications SDK enables real-time industrial communications for TI processors. Industrial communication is typically handled by the Programmable Real-Time Unit Industrial Communication Subsystem (PRU-ICSS). The PRU-ICSS is a co-processor subsystem containing Programmable Real-Time (PRU) cores and Ethernet media access controllers (EMACs), which implement the low level industrial Ethernet and fieldbus protocols through firmware. The upper layers of the protocols stacks are implemented in software running on ARM cores.

PRU cores are primarily used for industrial communication, and can also be used for other applications such as motor control and custom interfaces. The PRU-ICSS frees up the main ARM cores in the device for other functions, such as control and data processing.

Getting Started

To get started, see GETTING STARTED page.

Package Variants

The Industrial Communications SDK is provided in multiple package variants.

Variant prod eval
Standard x x
Premium x x
Premium Limited - x

License Types

There are different license types available. For details, read the license text in the corresponding installer. "eval" is only for evaluation and cannot be used for production. Some examples are only available in the Eval package. If you need some of these for production, there are further actions required. The "prod" package can be used for products without limitations.

Key differences between "eval" and "prod".

  • Beckhoff Library is not included in the production package. You can obtain the sources for free as an ETG member and need to compile it yourself in the production package.
  • The FSOE example is an evaluation version from Neuron Automation. In case you are interested in using it for production, please reach out to your TI sales contact.
  • The PROFIdrive example uses a reference implementation from PNO/Siemens. Please consult PNO/Siemens for the production usage.

Feature Variants

  • Standard is available for free on TI.com
  • Premium has additional features that are not free of charge. Features are also documented in the standard data sheets. If you are interested in using them, please contact your TI sales contact.
  • Premium Limited has the same feature set as Premium, but with a 1-hour runtime limitation. This is intended for customers who are interested in premium features and want to evaluate them. If you are interested, please contact your TI sales contact.

Support Model

For Standard packages, e2e support is provided. The support is limited to the contents in the SDK. Reported issues must be reproducible on TI EVMs. For premium, there is a private e2e forum available, which is handled on higher priority. On premium, there are also support hours for individual support included. On premium models, there is extended support for custom use cases possible.

Block Diagram

Given below is a block diagram of the software modules in this SDK

Software Block Diagram

The main software components in the block diagram are described below

Software Components Documentation Page Description
Device Drivers and HAL (Hardware Abstraction Layer)
Industrial Protocol Firmware (FW) HAL Industrial Communications FWHAL Hardware abstraction layer APIs to higher level industrial protocol stacks
Protocol Stacks and Middleware
Industrial Protocol Stacks Industrial Communications Toolkit Industrial protocol stacks for protocols like EtherCAT, Profinet, EtherNet/IP and IO-Link
Examples and Demos
Examples and Demos Examples and Demos Examples and demos showing usage of different software libraries and APIs

For details on software components of MCU+ SDK, please refer to AM261X MCU+ SDK.

Directory Structure

Given below is an overview of the directory structure to help you navigate the SDK and related tools.

Folder/Files Description
${SDK_INSTALL_PATH}/
README_FIRST_AM261X.html Open this file in a web browser to reach this user guide
makefile Top level makefile to build the whole SDK using "make"
imports.mak Top level makefile to list paths to dependent tools
docs/ Offline browseable HTML documentation
examples/ Example applications for AM261X, across multiple boards
source/ Device drivers, middleware libraries and APIs

Given below are the paths where the different tools needed outside the SDK, like CCS, SysConfig are installed by default in Windows. In Linux, the tools are installed by default in ${HOME}/ti.

Folder/Files Description
C:/ti/ccs2050 Code Composer Studio
C:/ti/sysconfig_1.27.0 SysConfig. NOTE, SysConfig is also installed as part of CCS at ${CCS_INSTALL_PATH}/ccs/utils/sysconfig_x.x.x
C:/ti/ti-cgt-armllvm_4.0.4.LTS TI ARM CLANG compiler tool chain

Licenses

The licensing information of this SDK, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed here [LINK] and the SDK Software License Agreement (SLA) is here [LINK]

Help and Support

For additional help and support, see https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum

Documentation Credits

This user guide is generated using Doxygen, see https://www.doxygen.nl/index.html