AM261x MCU+ SDK  10.02.00
TaskP.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2018-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef TASKP_H
34 #define TASKP_H
35 
36 #ifdef __cplusplus
37 extern "C" {
38 #endif
39 
40 #include <stdint.h>
41 #include <kernel/dpl/SystemP.h>
42 #if defined(__ARM_ARCH_7R__)
43 #include <kernel/dpl/MpuP_armv7.h>
44 #endif
45 
58 typedef void (*TaskP_FxnMain)(void *args);
59 
63 #define TaskP_PRIORITY_LOWEST (0u)
64 
68 #define TaskP_PRIORITY_HIGHEST (31u)
69 
73 #define TaskP_LOAD_UPDATE_WINDOW_MSEC (500u)
74 
75 
79 typedef struct {
80 
81  const char *name;
82  uint64_t runTime;
83  uint64_t totalTime;
84  uint32_t cpuLoad;
86 } TaskP_Load;
87 
91 #ifdef INCLUDE_FREERTOS_FAT
92 #define TaskP_OBJECT_SIZE_MAX (172u) /* Minimum requirement for FreeRTOS FATFS to work */
93 #elif MPU_FREERTOS
94 
96 #define TaskP_OBJECT_SIZE_MAX (4568u)
97 #else
98 #define TaskP_OBJECT_SIZE_MAX (160u)
99 #endif
100 
103 typedef struct TaskP_Object_ {
104 
105  /* uintptr_t translates to uint64_t for A53 and uint32_t for R5 and M4 */
106  /* This accounts for the 64bit pointer in A53 and 32bit pointer in R5 and M4 */
107  uintptr_t rsv[TaskP_OBJECT_SIZE_MAX/sizeof(uint32_t)];
109 } TaskP_Object;
110 
114 typedef struct TaskP_Params_ {
115 
116  const char *name;
117  uint32_t stackSize;
118  uint8_t *stack;
119  uint32_t priority;
120  void *args;
122  uintptr_t coreAffinity;
124 } TaskP_Params;
125 
126 #if defined(__ARM_ARCH_7R__)
127 
132 typedef struct TaskP_MpuRegionConfig_ {
133  uint32_t baseAddr;
134  uint32_t sizeBytes;
144  MpuP_RegionAttrs attrs;
145 } TaskP_MpuRegionConfig;
146 
152 typedef struct TaskP_ParamsRestricted_ {
153  TaskP_Params params;
154  TaskP_MpuRegionConfig regionConfig[7U];
155  // TODO: Replace with below after TaskP refactor to include FreeRTOS headers and structs directly.
156  // TaskP_MpuRegionConfig regionConfig[portNUM_CONFIGURABLE_REGIONS]; /**< MPU region configurations */
157 } TaskP_ParamsRestricted;
158 #endif
159 
168 
180 int32_t TaskP_construct(TaskP_Object *obj, const TaskP_Params *params);
181 
182 #if defined(__ARM_ARCH_7R__)
183 
192 void TaskP_ParamsRestricted_init(TaskP_ParamsRestricted *params);
193 
204 int32_t TaskP_constructRestricted(TaskP_Object *obj, const TaskP_ParamsRestricted *params);
205 #endif
206 
213 
214 
223 
227 void TaskP_yield(void);
228 
239 void TaskP_exit(void);
240 
247 void TaskP_loadGet(TaskP_Object *obj, TaskP_Load *taskLoad);
248 
260 
267 
268 
275 
278 #ifdef __cplusplus
279 }
280 #endif
281 
282 #endif /* TASKP_H */
TaskP_FxnMain
void(* TaskP_FxnMain)(void *args)
Entry point to the task.
Definition: TaskP.h:58
TaskP_Params
Parameters passed during TaskP_construct.
Definition: TaskP.h:114
args
void * args
Definition: hsmclient_msg.h:4
TaskP_Load
Task load statistics.
Definition: TaskP.h:79
SystemP.h
TaskP_Load::name
const char * name
Definition: TaskP.h:81
TaskP_Object
Opaque task object used with the task APIs.
Definition: TaskP.h:103
TaskP_loadResetAll
void TaskP_loadResetAll(void)
Reset task load statistics.
TaskP_Params::args
void * args
Definition: TaskP.h:120
TaskP_Params::name
const char * name
Definition: TaskP.h:116
TaskP_loadUpdateAll
void TaskP_loadUpdateAll(void)
Updated task load statistics.
TaskP_Params::taskMain
TaskP_FxnMain taskMain
Definition: TaskP.h:121
TaskP_exit
void TaskP_exit(void)
Exit current task.
MpuP_armv7.h
TaskP_yield
void TaskP_yield(void)
Yield current task.
TaskP_Params::stackSize
uint32_t stackSize
Definition: TaskP.h:117
TaskP_getHndl
void * TaskP_getHndl(TaskP_Object *obj)
Return OS defined task handle.
TaskP_Load::cpuLoad
uint32_t cpuLoad
Definition: TaskP.h:84
TaskP_Params::priority
uint32_t priority
Definition: TaskP.h:119
TaskP_construct
int32_t TaskP_construct(TaskP_Object *obj, const TaskP_Params *params)
Create a task object.
TaskP_loadGetTotalCpuLoad
uint32_t TaskP_loadGetTotalCpuLoad(void)
Get total CPU load including all task and ISR execution time.
TaskP_Load::runTime
uint64_t runTime
Definition: TaskP.h:82
TaskP_loadGet
void TaskP_loadGet(TaskP_Object *obj, TaskP_Load *taskLoad)
Get task load.
MpuP_RegionAttrs
Attribute's to apply for a MPU region.
Definition: MpuP_armv7.h:115
TaskP_Params::coreAffinity
uintptr_t coreAffinity
Definition: TaskP.h:122
TaskP_Load::totalTime
uint64_t totalTime
Definition: TaskP.h:83
TaskP_OBJECT_SIZE_MAX
#define TaskP_OBJECT_SIZE_MAX
Max size of task object across all OS's.
Definition: TaskP.h:98
TaskP_Params::stack
uint8_t * stack
Definition: TaskP.h:118
TaskP_Params_init
void TaskP_Params_init(TaskP_Params *params)
Set default values to TaskP_Params.
TaskP_destruct
void TaskP_destruct(TaskP_Object *obj)
Cleanup, delete, destruct a task object.