This example demonstrates the usage of the MCRC module. The example shows how to setup and use the MCRC controller in the auto mode of operation. Shows the generation of matching CRC as well as non-matching signature due to insertion of error in the block of information on which the CRC is being performed or in the signature provided to the PSA Signature Register (or both, depending on the mode).
| Use Case | Description |
|---|---|
| UC-1 | Auto CPU-mode signature compute for Channel 1 and comparison against known value. |
| UC-2 | Auto CPU-mode signature compute for Channel 2 and comparison against known value. |
Shown below is a sample output when the application is run,