AM261x MCU+ SDK  10.02.00
SDL ECC MSS L2

Introduction

This example demonstrates the usage of the SDL MSS L2 module. The example shows how to setup and use the ECC Safety Diagnostic operation. Shows the generation of SEC and DED error on MSS L2 ECC Aggregator.

Use Cases

Use Case Description
UC-1 Single bit error injection.
UC-2 Double bit error injection.

Supported Combinations

Steps to Run the Example

See Also

ECC : Error Correcting Code

Sample Output

Shown below is a sample output when the application is run,