AM261x MCU+ SDK  10.02.00
GPIO MULTI LED Blink

Introduction

This example configures multiple GPIO pins connected to LEDs on the EVM in output mode. The application toggles the each LED on/off for 10 seconds and exits.

Supported Combinations

Steps to Run the Example

See Also

GPIO

Sample Output

Shown below is a sample output when the application is run,

GPIO Multi LED Blink Test Started ...
Each LED will Blink for 10 seconds ...
GPIO Multi LED Blink Test Passed!!
All tests have passed!!