Introduction
ECAP APWM Phase Shift Feature.
This example showcases the phase shift feature of the ECAP.
Configurations,
- EPWM and 2 ECAPs (in APWM mode) are configured for period of 5000 SYSCLKs
- ECAPs are configured for Duty of 50% Active High PWM.
- ECAP 0 has phase shift value of 0, where are the ECAP1 has phase shift value of 2500.
- Output Xbars are used for routing the ECAP APWM output
External Connections
Observe ECAP outputs on the Outputxbar instances
AM263x
- CC E2, outputxbar 7,8 showcase ecap0,1 apwm outs respectively on HSEC pins 85 and 87
- LP, outputxbar 7,8 showcase ecap0,1 apwm outs respectively on J5.49, J5.50
AM263Px
- CC E2, outputxbar 7,8 showcase ecap0,1 apwm outs respectively on HSEC pins 85 and 87
- LP, outputxbar 7,8 showcase ecap0,1 apwm outs respectively on J5.49, J5.50
AM261x
- LP, outputxbar 1,5, showcase ecap 0,1 apwm outs respectively on J1.5, J5.48
- SOM E1, outputxbar 5,6 showcase ecap0,1 apwm outs respectively on HSEC pins 76 and 78
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Boards | am261x-som, am261x-lp |
| Example folder | examples/drivers/ecap/ecap_apwm_phase_shift/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
See Also
ECAP
Sample Output
Shown below is a sample output when the application is run,
ECAP APWM Phase Shift Test Started ...
ECAP APWM Phase Shift Test Passed!!
All tests have passed!!
Sample Output