AM261x INDUSTRIAL COMMUNICATIONS SDK  10.02.00
Profinet Device Demos

Introduction

Examples for Profinet Device IRT (Conformance Class - C) based on evaluation stacks provided in the SDK. Links to important sections in the detailed documentation are provided below:

Attention
If you need to reload and run the example again, EVM power-cycle is a MUST.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSM ICSSM0
Toolchain ti-arm-clang
Board am261x-lp
Example folder examples/industrial_comms/profinet_device_demo

See Also

Profinet Device FWHAL