Functions and callback-prototypes needed to handle ARs.
|
| typedef void(* | PN_API_IOD_reportArFsuRecordCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint8_t arFsuEnabled, const uint8_t arFsuChanged) |
| | Callback function prototype to notify the user application about an AR FSU update.
|
| |
| typedef void(* | PN_API_IOD_readyForInputUpdateCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint16_t arNum, const PN_API_IOD_InputUpdateState_t inputUpdateState) |
| | Callback function prototype to notify the user application that the stack is ready to receive the first valid input data.
|
| |
| typedef void(* | PN_API_IOD_arConnectCbf) (PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_ArType_t arType, uint32_t arNum, uint16_t sessionKey, uint16_t sendClock, uint16_t redRatioIoCrIn, uint16_t redRatioIoCrOut, uint32_t hostIpAddr) |
| | Callback function prototype to notify the user application that a new connection to an IO controller has been established.
|
| |
| typedef void(* | PN_API_IOD_arDisconnCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint16_t arNum, const uint16_t sessionKey, const PN_API_IOD_ArReason_t reasonCode) |
| | Callback function prototype to notify the user application that an AR connection with the IO controller has been terminated.
|
| |
| typedef void(* | PN_API_IOD_arOwnershipCbf) (PN_API_IOD_Handle_t *const pnHandle, uint32_t arNum, PN_API_IOD_Exp_t *ownSubmod) |
| | Callback function prototype to inform the user application about the submodule configuration assumed by the IO controller and to ask the IO device to claim the ownership of these submodules.
|
| |
| typedef PN_API_IOD_SubmodStatus_t(* | PN_API_IOD_paramEndCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint16_t arNum, const uint16_t sessionKey, const uint32_t api, const uint16_t slot, const uint16_t subslot, const bool moreFollows) |
| | Callback function prototype to notify the user application that the parameter assignment for all modules has been completed.
|
| |
| typedef void(* | PN_API_IOD_reportArFsuRecordCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint8_t arFsuEnabled, const uint8_t arFsuChanged) |
| | Callback function prototype to notify the user application about an AR FSU update.
|
| |
| typedef void(* | PN_API_IOD_readyForInputUpdateCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint16_t arNum, const PN_API_IOD_InputUpdateState_t inputUpdateState) |
| | Callback function prototype to notify the user application that the stack is ready to receive the first valid input data.
|
| |
| typedef void(* | PN_API_IOD_arConnectCbf) (PN_API_IOD_Handle_t *const pnHandle, PN_API_IOD_ArType_t arType, uint32_t arNum, uint16_t sessionKey, uint16_t sendClock, uint16_t redRatioIoCrIn, uint16_t redRatioIoCrOut, uint32_t hostIpAddr) |
| | Callback function prototype to notify the user application that a new connection to an IO controller has been established.
|
| |
| typedef void(* | PN_API_IOD_arDisconnCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint16_t arNum, const uint16_t sessionKey, const PN_API_IOD_ArReason_t reasonCode) |
| | Callback function prototype to notify the user application that an AR connection with the IO controller has been terminated.
|
| |
| typedef void(* | PN_API_IOD_arOwnershipCbf) (PN_API_IOD_Handle_t *const pnHandle, uint32_t arNum, PN_API_IOD_Exp_t *ownSubmod) |
| | Callback function prototype to inform the user application about the submodule configuration assumed by the IO controller and to ask the IO device to claim the ownership of these submodules.
|
| |
| typedef PN_API_IOD_SubmodStatus_t(* | PN_API_IOD_paramEndCbf) (PN_API_IOD_Handle_t *const pnHandle, const uint16_t arNum, const uint16_t sessionKey, const uint32_t api, const uint16_t slot, const uint16_t subslot, const bool moreFollows) |
| | Callback function prototype to notify the user application that the parameter assignment for all modules has been completed.
|
| |
|
| uint32_t | PN_API_IOD_arAbort (PN_API_IOD_Handle_t *const pnHandle, uint32_t arNum) |
| | A running application relationship to a PROFINET controller is terminated by this function.
|
| |
| PN_API_IOD_ArType_t | PN_API_IOD_arGetType (PN_API_IOD_Handle_t *const pnHandle, uint16_t arNum) |
| | Retrieves an application relation's type.
|
| |
|
#define | PN_API_IOD_ARFSU_ENABLED 0x01 |
| | FSU enabled.
|
| |
|
#define | PN_API_IOD_ARFSU_ENABLED 0x01 |
| | FSU enabled.
|
| |
|
#define | PN_API_IOD_ARFSU_DISABLED 0x00 |
| | FSU disabled.
|
| |
|
#define | PN_API_IOD_ARFSU_CHANGED 0x01 |
| | ARFSU_UUID changed in NV memory.
|
| |
|
#define | PN_API_IOD_ARFSU_NOT_CHANGED 0x00 |
| | ARFSU_UUID not changed in NV memory.
|
| |