Overview
The Sitara IO-Link master stack can be quickly integrated into supported devices
and helps to create IO-Link master applications on TI Sitara Embedded Processors with PRU-ICSS.
Licensing
Copyright © 2024, Texas Instruments Incorporated
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
-
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
-
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
-
Neither the name of the copyright holder nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Release Version 2.02.02
New Features:
-
[ICSTACK-383] Conformance to specification 1.1.4
-
[ICSTACK-382] add revision check for 1.0 devices.
Add more strict checks of DS content.
Add new error code ARGBLOCK_VALOUTOFRANGE.
Do not reconnect in case of PowerOn if it was already on.
-
[ICSTACK-392] set real revision ID for future revision in case of fault.
-
[ICSTACK-360] remove duplicated files of examples.
- Introduce board specific configuraton files.
- Introduce common and application specific files.
- Rename example files and folders.
- Renamed IOLM_LIB_getVersion to PRU_IOLM_getVersion. Stack API has not changed.
-
[ICSTACK-311] detect PRU frequency during initalization.
200MHz and 225MHz are supported.
Release Version 2.02.01
New Features:
-
[ICSTACK-228] Stack takes care for inital port power state. Last state is stored in non volatile memory.
NVM structure has changed. In case of reading data from older versions, it will be reset to defaults.
-
[ICSTACK-208] Add support for AM261.
The structure #IOLM_PL_sPortConfig_t has been extended for all targets to reflect PRU pin numbers for tx and rx.
Added option to switch the PRU0/1 function. By this it is also possible to use the GPIOs of PRU1 for rx/tx.
-
[ICSTACK-190] Added monitoring between R5 and PRU for cases where R5 misses frames. Detection may lead
to com errors, but no comlost. They are indicated by event 0x1F01 which could also be disabled.
Added API IOLM_SMI_psuGetInternalConfig for setting internal configuration. For details refer IOLM_SMasterCfg.
Stack Assertion are redirected to Error callback. See OSAL_registerErrorHandler. Critical error leads to sleep of
affected thread. Other threads can still do error handling.
Fixed Issues:
-
[ICSTACK-227] fixed hanging in case of PowerOffOn service during communication.
Added periphery mutex to prevent concurent access of different LEDs and EEPROM.
Release Version 2.02.00
New Features:
-
[ICSTACK-7] decreased stack sizes to actual needed values and reduce memory footprint
-
[ICSTACK-82] Support of AM263PX Launchpad
-
[OSS1-3071] Replaced LittleFS by direct access of EEPROM or Flash
Fixed Issues:
-
[ICSTACK-119] Latch of I/Q pin reading was missing in all example applications
Release Version 2.01.01
New Features:
-
[OSS1-3133] Migration to latest INDUSTRIAL-COMMUNICATIONS-SDK 09.02.
Fixed Issues:
-
[OSS1-3265] Fix pin2/IQ reads "not supported" after port-configuration.
Release Version 2.01.00
New Features:
-
[OSS1-3200] Update sysconfig files to use embedded linker.
Fixed Issues:
-
[OSS1-3195] Fix PDIn.PQI behavior for the port status: DI_C/Q and DO_C/Q.
Release Version 2.00.00
New Features:
-
[OSS1-712] IO-Link specification 1.1.3 Compliance for all boards.
-
[OSS1-2057] Added NVRAM support for AM243 LP and EVM in example app.
-
[OSS1-1726] Support for flexible Maximum number of Ports.
Fixed Issues:
-
[OSS1-2509] Correction of Port-Status value when no device is connected.
-
[OSS1-1684] Optimize FreeRTOS task priorities.
-
[OSS1-2034] Fix in the PRU to support TIOL112 Transceiver.
-
[OSS1-1885] Fixes to doxygen: disable dark mode.
Release Version 1.09.08
Fixed Issues:
-
[OSS1-924] IO-Link specification 1.1.3 conformance test case SDCI_TC_0158 TCM_PHYL_TIME_TDMT fix.
-
[OSS1-1761] IO-Link specification 1.1.3 conformance test case SDCI_TC_0354 TCM_ALIC_STOR_DELETEDSAFTERRECONF fix.
Release Version 1.09.07
Fixed Issues:
-
[OSS1-1363] Bugfix asynchronous NV-RAM write in IO-Link Sitara
Release Version 1.09.06
Fixed Issues:
-
[OSS1-1608] Path correction to "${INDUSTRIAL_COMMUNICATIONS_SDK_PATH}/mcu_plus_sdk"
Release Version 1.09.05
New Features:
-
[OSS1-1194] Updated MCU+SDK to 9.00.00.01 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+SDK.
-
[OSS1-928] Structure Alignment to other stacks.
-
[OSS1-720] AM64x/AM243x HSFS Upgrades.
-
[OSS1-869] Partial Conformity with IO-Link 1.13, ref. Known Issues for failing tests.
-
[OSS1-1202] Enable IOLM_PD_CYCLE_IRQ.
-
[OSS1-827] Implement roll-back if data storage upload failed.
-
[IOL8M-1293] IO-Link Master Release v1.08.00.
-
[OSS1-974] Implement non-volatile data storage in example application.
-
[OSS1-621] Upgrade to OSAL v1.1
-
[OSS1-888] Remove not needed event handling from the example.
-
[OSS1-730] Master start-up with overwrite of the RID (incompatible).
-
[OSS1-735] Master start-up with overwrite of the RID (compatible).
and Master start-up with incorrect DID (V1.0).
-
[OSS1-722] Feature/OSS1-722 implement corrigendum.
-
[OSS1-394] SMI header conversion.
-
[OSS1-535] Remove "nested interrupts" workaround.
Fixed Issues:
-
[IOL8M-1499] Port deactivated after power cycle.
-
[OSS1-925] Fix delay time of master messages.
-
[OSS1-745] Fix ISDU write response with illegal service code.
-
[OSS1-674] Fix multiple data storage issues.
-
[OSS1-678] Fix port event failures.
-
[OSS1-603] Fix memory footprint in documentation.
Release Version 1.09.04
New Features:
-
[IOL8M-1744] Updated MCU+ SDK to 8.05.00.24 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+ SDK.
-
[OSS1-413] Updated MCU+ SDK to 8.06.00.22 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+ SDK.
Fixed Issues:
-
[IOL8M-1629] Issues with nested Interrupts on MCU+SDK 8.05.00.01 for AM64x/AM243x.
The issue with nested interrupts has been resolved in 08.06.00.22. The issue
in previous versions could be corrected by:
To fix the issue comment out following line in
"source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos.c"
#define HWIP_NESTED_INTERRUPTS_IRQ_ENABLE
and rebuild the SDK.
Release Version 1.09.03
New Features:
-
[IOL8M-1737] Fix SMIExample state machine.
-
[IOL8M-1596] Add bug revision number.
-
[IOL8M-1607] Remove TIRTOS specific cmake commands
-
[IOL8M-1595] Remove customer specific code.
Release Version 1.09.02
New Features:
-
[IOL8M-1590] Updated MCU+SDK to 8.05.00.01 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+SDK.
Release Version 1.09.01
Release Version 1.09.00
New Features:
-
[IOL8M-1318] Updated MCU+ SDK to 8.04.00.01 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+ SDK.
Release Version 1.08.00
New Features:
-
[IOL8M-1272] Updated MCU+ SDK to 8.03.00.05 for AM64x/AM243x
Updated example projects to the latest MCU+ SDK.
Release Version 1.07.00
New Features:
-
[IOL8M-195] Test on AM243x EVM
AM243x EVM example has been successfully tested on AM243x EVM hardware.
-
[IOL8M-958] 400 us Cycle Time
Adjusted the IO-Link master to support IO-Link devices with a 400 us cycle time.
Currently, only one device with a 400 us cycle time can be guaranteed; further
testing will be required to verify that more than one device with a cycle time of
400 us can be supported.
-
[IMS-35] Wrong error code (IoLError_ServiceTempUnavailable)
When the port was correctly configured to output, the stack generated an incorrect
error code (IoLError_ServiceTempUnavailable). The corrected code is now
generated: IOLM_SMI_ePortStatus_DO_DQ.
Release Version 1.06.01
New Features:
-
[IOL8M-856] Reduced start-up time
Removed testing artefacts.
Release Version 1.06.00
New Features:
-
[IOL8M-291] FBTL SMI in Stack Support
The FBTL SMI support has been added.
-
[IOL8M-683] Uniform stack and heap size for FreeRTOS targets
Unified linker settings for AM243x and AM64x targets.
-
[IOL8M-279] Generic PL interface
Add interface to exchange PRU physical layer for IO-Link over SPI/UART/...
-
[IOL8M-810] Updated MCU+ SDK to 8.02.00.13 for AM64x/AM243x
Updated example projects to the latest MCU+ SDK.
Release Version 1.05.02
New Features:
-
[IOL8M-553] Updated MCU+ SDK to 8.01.00.35 for AM64x/AM243x
Updated example projects to the latest MCU+ SDK.
Release Version 1.05.01
Fixed Issues:
-
[IOL8M-460] Clean process removes needed parts
The install/unifdef process removed crucial parts in main.c,
due to major structural changes for the coming FBTL release.
Release Version 1.05.00
New Features:
-
[IOL8M-283] Complete Redesign of SMI Example
The SMI example has been completely revamped.
-
[IOL8M-295] Changed Example Stack access to SMI only
Low level non-SMI API has been removed.
-
[IOL8M-443] Page for Known Issues
The "Known Issues" listed in the release notes have been extracted and placed
into a new page in the documentation.
-
[IOL8M-455] Updated MCU+ SDK to 8.01.00.26 for AM64x/AM243x
Updated example projects to the latest MCU+ SDK.
Release Version 1.04.06
New Features:
-
[IOL8M-417] Updated MCU+ SDK to 8.01.00.15 for AM64x/AM243x
Minor release for doxygen Documentation
Release Version 1.04.05
New Features:
-
[IOL8M-312] Updated MCU+ SDK to 8.01.00.15 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+ SDK.
-
[IOL8M-296] Add RAM/ROM footprint to documentation for AM64x/AM243x
Updated documentation to include RAM and ROM usage of binaries.
Release Version 1.04.04
New Features:
-
[IOL8M-280] Updated MCU+ SDK to 8.01.00.10 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+ SDK.
-
[IOL8M-261] Move "Supported Functionality" to Top Level
The "Supported Functionality" section in the documentation has been moved from "General Information"
to the top-level.
Release Version 1.04.03
New Features:
-
[IOL8M-249] Added conformity reports for AM64x/AM243x
Included conformity reports in the AM64x EVM and AM243x Launchpad documentation.
Release Version 1.04.02
New Features:
-
[IOL8M-238] Updated MCU+ SDK to 8.01.00.02 for AM64x/AM243x
Updated example projects and documentation to the latest MCU+ SDK.
Release Version 1.04.01
Fixed Issues:
-
[IOL8M-227] Fix AM64x documentation
Minor error in AM64x documentation layout.
Release Version 1.04.00
New Features:
-
[IOL8M-211] Add AM243x Launchpad target
Added AM243x Launchpad target to project.
-
[IOL8M-214] IOLink GPIO mapping AM243x Launchpad
AM243x Launchpad GPIO Configuration for IOLink Booster.
-
[IOL8M-217] AM243x Launchpad UART SMI
SMI Interface over UART for Launchpad.
-
[IOL8M-220] AM243x Launchpad IOL-LED Porting
Added support for IOL status LEDs on IO expander.
Release Version 1.03.03
New Features:
-
[IOL8M-189] Add AM243x target
Added AM243x target to project.
Release Version 1.03.02
New Features:
-
[IOL8M-161] Conformity Tests AM64x
Passed IO-Link Master conformity tests with AM64x EVM hardware.
Fixed Issues:
-
[IOL8M-166] HwiP problems on AM64x
Fixed exceptions when working with hardware interrupts.
-
[IOL8M-167] Assertion in IO-Link Stack
Fixed buffer overflow in event ring buffer.
Release Version 1.03.01
New Features:
-
[IOL8M-64] IQ Service AM65x
Implemented IQ Input service on AM65x EVM board.
Release Version 1.03.00
New Features:
-
[IOL8M-101] LED Port
The LEDS on the IOLink/Breakout board have been ported to the AM64x and are correctly signaling the port status.
-
[IOL8M-129] PRU IRQ Mapping
IRQs from the PRU are now registered in the backend for the AM64x.
-
[IOL8M-125] PRU Backend Porting
Established communication between the PRU backend and the PRU for the AM64x.
-
[IOL8M-123] OSAL FreeRTOS tasks
Implemented FreeRTOS task execution for the AM64x.
-
[IOL8M-112] OSAL FreeRTOS initialization.
Implemented initialization routine for FreeRTOS on the AM64x.
Fixed Issues:
-
[IOL8M-158] SMI over UART
Standardized Master Interface (SMI) can now be controlled on the AM64x via UART.
-
[IOL8M-114] Exception when booting up AM65x.
Corrected exception issue caused by calling incorrect stack reference.
Release Version 1.02.02
New Features:
-
[IOL8M-108] Configurable DO mode option.
Added PNP/NPN/Push-Pull-Switch possibility for CQ signal driver in SIO mode.
Release Version 1.02.01
New Features:
-
Standardized Master Interface accessible via UART Connector J42 on AM65x EVM.
-
LED Configuration management provided to Application.
Release Version 1.01.01
New Features:
-
Project structure cleanup
Fixed Issues:
-
Bugfix in Wakeup procedure
Release Version 1.01.00
New Features:
-
Standards supported by this Release are:
IO-Link Stack according to IEC 61131-9 Spec V1.1
IODD V1.1
-
Functions supported by this Release are:
IO-Link Master Stack
Standard Master Interface
-
Communication Classes supported are:
Com1, Com2, Com3 (4.8, 38.4, 230.4 Kbps)
-
Telegram Types supported are:
0, 1, 2.1, 2.2, 2.3, 2.4, 2.5
-
This Release supports up to 8 IO-Link Channels in parallel.