IO-Link Master2.02.04
 
Loading...
Searching...
No Matches
Introduction

This is the integration manual of the IO-Link® Master stack including an example application.

To communicate with the IO-Link stack library use SMI - The Standardized Master Interface (SMI). It is a generic interface, which is set on top of the stack's regular API. It matches the interface with other IO-Link standards and acts as a connecting interface for multiple clients. It also includes the configuration management and event dispatching.