| Feature |
|---|
| PROFIdrive Example (premium only) |
| PROFINET VLAN Filtering Support |
| FSOE example |
| IO-Link FWHAL |
| HSR Layer 2 1G Example |
| HSR 1G: PTP over HSR support (Only PRU firmware support) |
| PRP 1G: PTP over PRP support (Only PRU firmware support) |
| PROFINET RGMII Support |
| SOC | Supported CPUs | Boards | Host PC |
|---|---|---|---|
| AM243x | R5F | AM243x GP EVM (referred to as am243x-evm in code), AM243x LAUNCHPAD (referred to as am243x-lp in code) | Windows 11 64b or Ubuntu 22.04 64b or MacOS |
| Tools / SW module | Supported CPUs | Version |
|---|---|---|
| Code Composer Studio | R5F, M4F | 20.4.0 |
| SysConfig | R5F, M4F | 1.26.0, build 4407 |
| TI ARM CLANG | R5F, M4F | 4.0.4.LTS |
| MCU-PLUS-SDK-AM243X | R5F, M4F | 12.00.00.26 |
| FreeRTOS Kernel | R5F, M4F | 11.1.0 |
| Tiny USB | R5F | 0.14.0 |
| LwIP | R5F | STABLE-2_2_1_RELEASE |
| Mbed-TLS | R5F | mbedtls-2.13.1 |
| ID | Head Line | Module | Applicable Releases | Resolution/Comments |
|---|---|---|---|---|
| PINDSW-8517 | SYNC1 Generated 1 cycle after first SYNC0 pulse when SYNC1 shift is configured from MainDevice | EtherCAT SubDevice | 09.02.00 | More details in EtherCAT SubDevice Errata |
| PINDSW-9560 | TX_START_DELAY reset to default value when link broken and re-connected to the network during OP | EtherCAT SubDevice | 2025.00.00 | More details in EtherCAT SubDevice Errata |
| PINDSW-9756 | CRC/Alignment Error observed when one SubDevice set to INIT after link re-connection | EtherCAT SubDevice | 2025.00.00 | More details in EtherCAT SubDevice Errata |
| PINDSW-9787 | CRC Error for 8SM application individual SubDevice state transition to INIT | EtherCAT SubDevice | 2025.00.00 | More details in EtherCAT SubDevice Errata |
| PINDSW-9821 | Malformed packet formation for 1 byte mailbox data communication due to cycle budget | EtherCAT SubDevice | 2025.00.00 | More details in EtherCAT SubDevice Errata |
| PINDSW-9883 | PDO misalignment due to start offset in FMMU merge logic for LRD/LWR | EtherCAT SubDevice | 2025.00.00 | More details in EtherCAT SubDevice Errata |
| PINDSW-9909 | Add support for ESI EEPROM over SPI Flash | EtherCAT SubDevice | 2025.00.00 | Refer to ESI EEPROM over SPI Flash |
| PINDSW-10013 | Use bsp_global_mutex_lock_save and bsp_global_mutex_restore in place of HwiP_disable and HwiP_restore | EtherCAT SubDevice | 2025.00.00 | |
| PINDSW-10185 | Fix build errors due to Beckhoff stack source patch script error | EtherCAT SubDevice | 2025.00.00 | |
| PINDSW-10390 | Add support for configuring TX_CLK_DELAY in the forward path | EtherCAT SubDevice | 2025.00.00 | Refer to TIESC_PROCESS_PATH_TX_CLK_DELAY in tiescbsp.h |
| PINDSW-8498 | PPM frames transmit with incorrect cycle counter | PROFINET Device | 11.00.00 | |
| PINDSW-9608 | HSR 1G: Host receives duplicate PTP frames due to duplicate discard check | HSR | 2025.00.00 | RX L2 filter used to classify incoming PTP frames; duplicate discard check is skipped for PTP packets |
| PINDSW-10236 | PRP 1G: PTP packets incorrectly subject to duplicate discard and TX duplication | PRP | 2025.00.00 | Duplicate discard and TX duplicate logic skipped for PTP packets over PRP |
| PINDSW-10261 | PRP 1G: Host receives duplicate PTP frames due to duplicate discard check | PRP | 2025.00.00 | RX L2 filter used to classify incoming PTP frames; duplicate discard check is skipped for PTP packets |
| PINDSW-10285 | HSR sequence counter not SYNC between RTU | HSR | 2025.00.00 | HSR sequence counter synchronized between RTUs to prevent out-of-sequence packets |
| PINDSW-10289 | ICSSG: transmit queue timed out when 10M link is unplugged repeatedly | HSR | 2025.00.00 | |
| PINDSW-10291 | PRP sequence counter not SYNC between RTU | PRP | 2025.00.00 | PRP sequence counter synchronized between RTUs to prevent out-of-sequence packets |
| ID | Head Line | Module | Applicable Releases | Workaround |
|---|---|---|---|---|
| PINDSW-5666 | EtherNet/IP : PTP Device is unable to keep offset under 1000 ns | EtherNet/IP Adapter | 08.04.00 | Value of OFFSET_THRESHOLD_FOR_RESET is set to 10000 ns by default in SDK |
| PINDSW-8333 | Provide option for setting Sync ISR (FIQ) flag to reduce latency on SYNC0 interrupt | EtherCAT SubDevice | 10.02.00 | Modify PRUICSS_registerIrqHandler in mcu_plus_sdk\source\drivers\pruicss\g_v0\pruicss_g_v0.c with an additional argument for setting/unsetting FIQ: --- a/source/drivers/pruicss/g_v0/pruicss.h
+++ b/source/drivers/pruicss/g_v0/pruicss.h
@@ -451,6 +451,7 @@ int32_t PRUICSS_registerIrqHandler(PRUICSS_Handle handle,
int32_t intrNum,
int32_t eventNum,
uint8_t waitEnable,
+ uint8_t isFIQFlagSet,
PRUICSS_IrqHandler irqHandler);
/**
diff --git a/source/drivers/pruicss/g_v0/pruicss_g_v0.c b/source/drivers/pruicss/g_v0/pruicss_g_v0.c
index 2531e915..e37bf610 100644
--- a/source/drivers/pruicss/g_v0/pruicss_g_v0.c
+++ b/source/drivers/pruicss/g_v0/pruicss_g_v0.c
@@ -279,6 +279,7 @@ int32_t PRUICSS_registerIrqHandler(PRUICSS_Handle handle,
int32_t intrNum,
int32_t eventNum,
uint8_t waitEnable,
+ uint8_t isFIQFlagSet,
PRUICSS_IrqHandler irqHandler)
{
PRUICSS_Object *object;
@@ -311,6 +312,7 @@ int32_t PRUICSS_registerIrqHandler(PRUICSS_Handle handle,
/*TODO: Take priority as an argument to this function*/
hwiParams.priority = 0x1;
hwiParams.intNum = intrNum;
+ hwiParams.isFIQ = isFIQFlagSet;
hwiParams.callback = (HwiP_FxnCallback)PRUICSS_hwiIntHandler;
retVal = HwiP_construct(&(object->pruEvntOutFnMapArray[pruEvtoutNum].hwiObj), &hwiParams);
gmake -s -f makefile.am243x drivers_r5f.ti-arm-clang.freertos PROFILE=debug
gmake -s -f makefile.am243x drivers_r5f.ti-arm-clang.freertos PROFILE=release
|
| PINDSW-10802 | PROFINET: Startup issues with RGMII application in ART regression | PROFINET Device | 2026.00.00 | Re-run specific test case |
| PINDSW-10803 | PROFINET: Sporadic SPIRTA failures observed in RGMII application | PROFINET Device | 2026.00.00 | Re-run specific test case. |
This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.
| Module | Affected API | Change | Additional Remarks |
|---|---|---|---|
| EtherNet/IP Adapter Demo | N/A | Refactor folder structures and naming convention for the Examples. | Refer to Overview of EtherNet/IP Adapter Demo |
| Module | Affected API | Change | Additional Remarks |
|---|