EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches
EC_API_SLV_CoE_ObjEntry Struct Reference

#include <ecSlvApiInternal.h>

Data Fields

uint16_t index
 Object Index number.
 
uint8_t subIndex
 Object SubIndex number.
 
uint8_t rsvd
 alignment
 
char * pName
 Object entry name.
 
uint8_t * pVarPtr
 Pointer to data memory space.
 
uint32_t enumValue
 Enum Value.
 
void * enumMemory
 Enum Memory area.
 
TSDOINFOENTRYDESC * pSdoEntryInfo
 Object entry descriptor.
 
struct EC_API_SLV_CoE_ObjEntry * pNext
 Pointer to next entry.
 

Detailed Description