EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_load()

uint32_t EC_API_SLV_load ( OSAL_ERR_CBHandler_t  cbErrHandler,
uint32_t  pruSelect 
)

Initialize stack environment (OSAL and HWAL) after load.

Parameters
[in]cbErrHandlerException callback
[in]pruSelectselection of logical PRU (1,2,...)
Returns
0 on success, errorcode otherwise
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
// the Call
retVal = uint32_t retVal = EC_API_SLV_Load(applErrHandler, EC_API_SLV_ePRUICSS_INSTANCE_ONE);
@ EC_API_SLV_ePRUICSS_INSTANCE_ONE
Definition ecSlvApi_types.h:53
See also
EC_API_SLV_UnLoad
Examples
EtherCAT_SubDevice_CiA402.c, EtherCAT_SubDevice_Simple.c, and EtherCAT_SubDevice_Webserver.c.