EtherCAT SubDevice
2.03.00
Loading...
Searching...
No Matches
◆
EC_SLV_APP_FoE_fileWrite()
uint32_t EC_SLV_APP_FoE_fileWrite
(
void *
pContext
,
uint16_t *
pData
,
uint16_t
size
)
Write file from device.
Parameters
[in]
pContext
context
[in]
pData
Data Buffer.
[in]
size
write length parameter.
Returns
ErrorCode FoE error code.
Example
// required variables
uint16_t* pData;
uint16_t length;
// the Call
retVal =
EC_SLV_APP_FoE_fileWrite
(pData, length);
EC_SLV_APP_FoE_fileWrite
uint32_t EC_SLV_APP_FoE_fileWrite(void *pContext, uint16_t *pData, uint16_t size)
Write file from device.
Definition
ESL_foeDemo.c:363
File access over EtherCAT functions
generated by
1.9.8