| bool EC_SLV_APP_EoE_SS_settingIndHandler | ( | void * | pContext, |
| uint16_t * | pMac, | ||
| uint16_t * | pIp, | ||
| uint16_t * | pSubNet, | ||
| uint16_t * | pDefaultGateway, | ||
| uint16_t * | pDnsIp | ||
| ) |
EoE Settings Indication callback. Called when EoE settings are received.
| [in] | pContext | The pointer to the application instance. |
| [in] | pMac | Virtual Net MAC address |
| [in] | pIp | Virtual Net IP address |
| [in] | pSubNet | Virtual Net Subnet |
| [in] | pDefaultGateway | Virtual Net Default Gateway |
| [in] | pDnsIp | Virtual Net DNS server address |