EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_SLV_APP_EoE_SS_receiveHandler()

bool EC_SLV_APP_EoE_SS_receiveHandler ( void *  pContext,
uint16_t *  pData,
uint16_t  size 
)

User defined EoE receive function. Called when an EoE frame is received.

Parameters
[in]pContextfunction context
[in]pDataEoE Frame Data
[in]sizeEoE Frame Size
Returns
true if frame is handle, false if it should be passed on.