Functions | |
| void | EC_SLV_APP_EEP_init (void *pContext) |
| Initialize EEPROM instance. | |
| void | EC_SLV_APP_EEP_write (void *pContext, void *pEeprom, uint32_t length) |
| Write EEPROM to memory. | |
| bool | EC_SLV_APP_EEP_read (void *pContext, void *pEeprom, uint32_t *pLength) |
| Load EEPROM from memory. | |
| bool | EC_SLV_APP_EEP_getMacAddress (void *pMagicKey, uint8_t *pMacAddress) |
| Retrieves the MAC address from the EEPROM. | |
| bool | EC_SLV_APP_EEP_getBoardRevision (void *pMagicKey, uint8_t *pBoardRevision) |
| Retrieves the board revision information from the EEPROM. | |