| uint32_t EC_API_SLV_VoE_cbRegisterManualTestHandler | ( | EC_API_SLV_SHandle_t * | pHandle, |
| EC_API_SLV_VoE_CBTestHandler_t | cbFunc, | ||
| void * | pContext | ||
| ) |
Function to register a VoE manual inject test handler.
This function registers a function pointer which must be implemented by the user. The user defined function will be called periodically based on the configuration defines in ecat_def.h.
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | cbFunc | Function pointer to the VoE manual test handler. |
| [in] | pContext | VoE initHandler call context. |