EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_cbRegisterStopOuputHandler()

uint32_t EC_API_SLV_cbRegisterStopOuputHandler ( EC_API_SLV_SHandle_t *  pHandle,
EC_API_SLV_CBStopOutputHandler_t  cbFunc,
void *  pContext 
)

This is the function to register a function which stops the output handler.

The function is called in the state transition from OP to SAFEOP to stop the output handler. This functions informs the application about the state transition, the application cannot refuse the state transition

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]cbFuncFunction pointer to the Stop Output Handler
[in]pContextstopOutputHandler call context
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// the Call
uint32_t EC_API_SLV_cbRegisterStopOuputHandler(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_CBStopOutputHandler_t cbFunc, void *pContext)
This is the function to register a function which stops the output handler.
Definition ecSlvApi_ssc.c:393