| uint32_t EC_API_SLV_PDO_getPdoType | ( | EC_API_SLV_SHandle_t * | pHandle, |
| EC_API_SLV_Pdo_t * | pPdo, | ||
| uint8_t * | pPdoType | ||
| ) |
Get the PDO type.
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | pPdo | pointer to PDO instance. |
| [out] | pPdoType | pointer to memory to where the PDO type is copied. 'True' if PDO is a TxPDO, 'False' if PDO is a RxPDO. |