EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_PDO_registerAssignmentChanges()

uint32_t EC_API_SLV_PDO_registerAssignmentChanges ( EC_API_SLV_SHandle_t *  pHandle,
EC_API_SLV_PDO_CBAssignmentChanges_t  cbFunc,
void *  pContext 
)

Report PDO assignment changes.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]cbFuncFunction pointer to the PDO assignment changes.
[in]pContextPDO assignment changes call context.
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_cbRegisterAssignmentChanges(pHandle, pContext, cbFunc);
Examples
ecSubDeviceSimple.c.