EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_PDO_registerMappingChanges()

uint32_t EC_API_SLV_PDO_registerMappingChanges ( EC_API_SLV_SHandle_t *  pHandle,
EC_API_SLV_PDO_CBMappingChanges_t  cbFunc,
void *  pContext 
)

Report PDO mapping changes.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]cbFuncFunction pointer to the PDO assignment changes.
[in]pContextPDO mapping changes call context.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_PDO_registerMappingChanges(pHandle, pContext, cbFunc);
uint32_t EC_API_SLV_PDO_registerMappingChanges(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_PDO_CBMappingChanges_t cbFunc, void *pContext)
Report PDO mapping changes.
Definition ecSlvApi_pdo.c:2949
Examples
ecSubDeviceSimple.c.