EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_getInputProcDataLength()

uint32_t EC_API_SLV_getInputProcDataLength ( EC_API_SLV_SHandle_t *  pHandle,
uint32_t *  pLength 
)

Read the input process data length.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[out]pLengthinput process data length in bits.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
uint32_t length = EC_API_SLV_getInputProcDataLength(ptEcSlvApi);
uint32_t EC_API_SLV_getInputProcDataLength(EC_API_SLV_SHandle_t *pHandle, uint32_t *pLength)
Read the input process data length.
Definition ecSlvApi_pdo.c:1995
See also
EC_API_SLV_getOutputProcDataLength
Examples
ESL_cia402Demo.c.