EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_FoE_cbRegisterReadFileHandler()

uint32_t EC_API_SLV_FoE_cbRegisterReadFileHandler ( EC_API_SLV_SHandle_t *  pHandle,
EC_API_SLV_FoE_CBReadFileHandler_t  cbFunc,
void *  pContext 
)

This is the function to register FoE read function.

This function registers a function pointer which must be implemented by the user. The user defined function will be called if a file read request is received from the master.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]cbFunccbFunc Function pointer to the FoE Read file
[in]pContextreadFileHandler call context
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_FoE_cbRegisterReadFileHandler(ecSlaveApi, cbFunc, pCtxt);
uint32_t EC_API_SLV_FoE_cbRegisterReadFileHandler(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_FoE_CBReadFileHandler_t cbFunc, void *pContext)
This is the function to register FoE read function.
Definition ecSlvApi_FoE.c:94
Examples
ecSubDeviceSimple.c.