EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_FoE_cbRegisterStartBLHandler()

uint32_t EC_API_SLV_FoE_cbRegisterStartBLHandler ( EC_API_SLV_SHandle_t *  pHandle,
EC_API_SLV_FoE_CBStartBLHandler_t  cbFunc,
void *  pContext 
)

This is the function to register FoE bootloader start function.

This function registers a function pointer which must be implemented by the user. The user defined function will be called during the state transition from INIT to BOOTSTRAP mode.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]cbFuncFunction pointer to the FoE BL start Handler
[in]pContextBLStartHandler call context
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_FoE_cbRegisterStartBLHandler(ecSlaveApi, cbFunc, pCtxt);
uint32_t EC_API_SLV_FoE_cbRegisterStartBLHandler(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_FoE_CBStartBLHandler_t cbFunc, void *pContext)
This is the function to register FoE bootloader start function.
Definition ecSlvApi_FoE.c:218
Examples
ecSubDeviceSimple.c.