EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_setFwUpdateMode()

uint32_t EC_API_SLV_setFwUpdateMode ( EC_API_SLV_SHandle_t *  pHandle,
bool  fwUpdateRequired 
)

Set whether firmware update is required after file read via FoE.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]fwUpdateRequiredFirmware update required
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_setFwUpdateMode(ecSlaveApi, false);
uint32_t EC_API_SLV_setFwUpdateMode(EC_API_SLV_SHandle_t *pHandle, bool fwUpdateRequired)
Set whether firmware update is required after file read via FoE.
Definition ecSlvApi_FoE.c:377