| uint32_t EC_API_SLV_ESI_parseFileRam | ( | EC_API_SLV_SHandle_t * | pHandle, |
| const uint8_t * | pData_p, | ||
| uint32_t | length_p | ||
| ) |
Parse an ESI file from a RAM source.
This function is used to parse an ESI file from a RAM source.
| pHandle | Pointer to the EC_API_SLV_SHandle_t structure. |
| pData_p | Pointer to the start of the RAM data. |
| length_p | Length of the RAM data. |