| uint32_t EC_API_SLV_CoE_getObjectLengthByIndex | ( | EC_API_SLV_SHandle_t * | pHandle, |
| uint16_t | index, | ||
| uint32_t * | length | ||
| ) |
This function returns the object length including subIndex 0.
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | index | Object index |
| [out] | length | object size. |