| uint32_t EC_API_SLV_CiA402_getAllDriveFunctionStatus | ( | EC_API_SLV_SHandle_t * | pHandle, |
| uint8_t | axisNo, | ||
| uint8_t * | driveFunctionStatus | ||
| ) |
Get all CiA402 drive function status encoded into byte.
| [in] | pHandle | SubDevice API Handle Instance |
| [in] | axisNo | Number of Axis. |
| [out] | drivefunction | all drive function status encoded into byte. |