EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_CiA402_setAxisNumber()

uint32_t EC_API_SLV_CiA402_setAxisNumber ( EC_API_SLV_SHandle_t *  pHandle,
uint8_t  axisNo 
)

Set number of CiA402 axis configured.

Parameters
[in]pHandleSubDevice API Handle Instance
[in]axisNoNumber of Axis.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint8_t axisNo;
// the Call
EC_API_SLV_CiA402_setAxisNumber(S_ecSlvApiHdl, AxisNo);
uint32_t EC_API_SLV_CiA402_setAxisNumber(EC_API_SLV_SHandle_t *pHandle, uint8_t axisNo)
Set number of CiA402 axis configured.
Definition ecSlvApi_CiA402.c:258
Definition ecSlvApiInternal.h:351
Examples
ecSubDeviceCiA402.c.