| uint32_t EC_API_SLV_CiA402_registerStateMachine | ( | EC_API_SLV_SHandle_t * | pHandle, |
| EC_API_SLV_CiA402_CBUsrApplSM_t | cbFunc, | ||
| void * | pContext | ||
| ) |
Set User defined CiA402 State Machine.
If not set, an internal state machine is provided by the DTK.
| [in] | pHandle | SubDevice API Handle Instance |
| [in] | cbFunc | Handle for user defined CiA402 State Machine. |
| [in] | pContext | CiA402 stateMachine call context |