| uint32_t EC_API_SLV_CiA402_SM_clearErrorCode | ( | EC_API_SLV_SHandle_t * | pHandle, |
| uint8_t | axisNo | ||
| ) |
Set error code on axis.
User CiA402 must inform regarding the error option codes, the state machine requires input from the application. For example, if a Quick Stop was triggered, the SM has to be informed whether the QS action finished or it is still pending to finish.
| [in] | pHandle | SubDevice API Handle Instance |
| [in] | axisNo | Number of Axis. |