EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_CiA402_activateAxis()

uint32_t EC_API_SLV_CiA402_activateAxis ( EC_API_SLV_SHandle_t *  pHandle,
uint8_t  axisNo,
bool  active 
)

Activate Axis.

Parameters
[in]pHandleSubDevice API Handle Instance
[in]axisNoAxis number.
[in]activeactivate axis.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint8_t axisNo;
bool active;
// the Call
EC_API_SLV_CiA402_activateAxis(S_ecSlvApiHdl, axisNo, active);
uint32_t EC_API_SLV_CiA402_activateAxis(EC_API_SLV_SHandle_t *pHandle, uint8_t axisNo, bool active)
Activate Axis.
Definition ecSlvApi_CiA402.c:349
Definition ecSlvApiInternal.h:351
Examples
ESL_cia402Demo.c.