EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_CiA402_getAxisActivateStatus()

uint32_t EC_API_SLV_CiA402_getAxisActivateStatus ( EC_API_SLV_SHandle_t *  pHandle,
uint8_t  axisNo,
uint8_t *  status 
)

Get Axis Activate status.

Parameters
[in]pHandleSubDevice API Handle Instance
[in]axisNoNumber of Axis.
[out]status'True' if Axis is activated otherwise 'False'.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint8_t axisNo;
uint8_t status;
// the Call
EC_API_SLV_CiA402_getAxisActivateStatus(S_ecSlvApiHdl, axisNo, &status);
uint32_t EC_API_SLV_CiA402_getAxisActivateStatus(EC_API_SLV_SHandle_t *pHandle, uint8_t axisNo, uint8_t *status)
Get Axis Activate status.
Definition ecSlvApi_CiA402.c:387
Definition ecSlvApiInternal.h:351
Examples
ESL_cia402Demo.c.