EtherCAT SubDevice2.03.00
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_setPDICfg()

uint32_t EC_API_SLV_setPDICfg ( EC_API_SLV_SHandle_t *  pHandle,
uint16_t  pdiControl,
uint16_t  pdiConfig 
)

Set PDI Configuration.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]pdiControlEC_API_SLV_SEeprom_t PDI Control.
[in]pdiConfigEC_API_SLV_SEeprom_t PDI Config.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_setPDICfg(S_ecSlvApiHdl, 0x0C80, 0x88E0);
uint32_t EC_API_SLV_setPDICfg(EC_API_SLV_SHandle_t *pHandle, uint16_t pdiControl, uint16_t pdiConfig)
Set PDI Configuration.
Definition ecSlvApi_param.c:587
Definition ecSlvApiInternal.h:351
Examples
ecSubDeviceCiA402.c.